Change Language :
Rotary and indexing motion plays a critical role throughout modern machine tools, from tool changers and operator controls to auxiliary rotary tables, indexing fixtures, pallet systems, belt drives, and automated machine tending cells. These movements may rotate continuously, index between fixed positions, swivel through a limited angle, or repeatedly reposition parts and components within the machine or between processes. Selecting the right rotary motion components depends on load, speed, accuracy, rotation angle, duty cycle, installation space, contamination, and cable or hose routing requirements.
igus® offers a broad range of components for supporting rotary and indexing motion, including PRT slewing ring bearings, drygear® rotary drives, igubal® self-aligning bearings, xiros® ball bearings, custom polymer gears, and rotary cable management systems. These dry-running solutions help reduce maintenance and simplify assemblies in machine tool environments exposed to chips, coolant, dust, vibration, and repeated cycling. PRT slewing ring bearings provide an open center, while drygear® RL-D worm gear drives feature a central bore for cable or hose feed-through, creating options for routing utilities directly through rotary assemblies.
There is no single best component for every rotary application. Start with what is rotating, the applied load, required speed, positioning accuracy, duty cycle, and operating environment. The bearing or drive should follow the actual motion and load path rather than the fact that the assembly rotates.
For supporting machine motion, common igus® options include PRT slewing ring bearings for combined axial, radial, and moment loads; drygear® gearboxes for driven positioning and indexing; igubal® self-aligning bearings where misalignment must be accommodated; and xiros® ball bearings for lighter, lower-friction rotary motion.
Primary fourth- and fifth-axis machining tables are a different class of system. They are selected around machining accuracy, repeatability, stiffness, feedback, and performance under cutting load, while igus® is strongest in supporting rotary and indexing motion inside and around the machine or automation cell.
Rotary and indexing motion appears throughout modern machine tools, not only at the main machining axis. Supporting systems rotate, swivel, pivot, or index to position tools, controls, workpieces, sensors, and automation equipment.
Common examples include automatic tool changers and tool magazines, swiveling operator panels, auxiliary rotary tables, indexing fixtures, belt drives, pallet handling, machine tending, inspection equipment, and rotary cable or hose guidance. In automated machining cells, rotary motion can also help orient, present, and transfer parts between machines or process steps. The motion may be continuous, limited-angle, or indexed between defined positions depending on the machine function.
Rotary motion is the broad category for components or assemblies that turn around an axis. The movement may be continuous, such as a pulley or shaft, or limited to a defined swivel angle. Indexing motion is a type of rotary motion in which the system moves to a specific angular position, stops or dwells, performs a task, and then moves to the next position.
For a machine tool designer, the key questions are whether the application needs continuous rotation or discrete positions, how accurately it must stop, whether mechanical locking is required, and whether the movement supports the cutting process or the machine around it. These answers determine whether a simple bearing and drive, a geared rotary mechanism, or a precision servo-driven rotary table is appropriate.
Rotary and indexing mechanisms are selected around accuracy, speed, torque, positioning flexibility, duty cycle, stiffness, and cost. Direct-drive torque motors, cam indexers, servo-driven rotary tables, worm gear drives, roller gear drives, and strain wave systems each occupy different performance ranges.
A slewing ring bearing is useful when a broad rotary interface must carry combinations of axial, radial, and moment loads. That makes slewing rings a strong fit for supporting applications such as operator controls, turntables, machine tending systems, rotary fixtures, and other swivel or positioning assemblies.
A crossed-roller, YRT, thin-section, or other high-stiffness precision bearing arrangement may be more appropriate when the rotary axis is part of the actual cutting process and requires very high stiffness and quantified machining accuracy. For auxiliary motion, PRT can provide a compact dry-running alternative with gearing, locking, and angle-limiting options available across the family.
Machine tool environments can expose supporting rotary assemblies to chips, metal debris, dust, coolant splash, and repeated cycling. Component material and sealing requirements should always be checked against the actual exposure, load, speed, and temperature.
Dry-running polymer components can reduce maintenance because they do not rely on an externally applied grease film that can collect contamination. Depending on the movement, options include PRT slewing ring bearings, igubal® self-aligning bearings, xiros® ball bearings, and 3D-printed polymer gears for suitable supporting applications.
Cable routing should be considered part of the rotary assembly from the beginning, not added after the bearing and drive are already selected. The correct approach depends on the total rotation angle, available space, cable type, bend radius, torsion capability, and whether the motion is continuous or limited-angle.
For limited rotation, a controlled cable loop or suitable rotary e-chain® system can guide power, data, air, and other media while controlling bend radius and preventing uncontrolled twisting. Hollow-center bearings or gearboxes can also create a useful cable feed-through path. For unrestricted continuous rotation, a slip ring or rotary union may still be required depending on the media being transferred.
The positioning method should match the accuracy the application actually needs. Supporting rotary motion may use mechanical stops, angle limiters, detents, hand-adjustable locks, sensors, or motor control to define or hold a position.
More demanding CNC rotary tables may use absolute encoders, servo feedback, hydraulic or pneumatic clamps, and other precision positioning hardware. For auxiliary machine motion, simpler mechanisms can reduce complexity and cost when machining-grade repeatability is not required. PRT slewing ring bearings offer configurations with angle-limiting, locking, and geared options for suitable applications.
Not every indexing application requires a servo. A servo-driven rotary system is valuable when the application requires programmable positions, feedback, controlled acceleration, or tighter positioning accuracy. Simpler supporting movements may use stepper motors, worm gear drives, mechanical stops, sensors, or other lower-complexity positioning methods.
The right approach depends on how accurately the system must position, how often positions change, the required speed and torque, and whether the movement is part of the machining process or supporting automation. For auxiliary indexing, using only the level of control the application actually requires can reduce cost and system complexity.
Tool changers and machine tending systems often need reliable rotary or indexing motion without the same accuracy requirements as the primary machining axis. The right solution depends on whether the system is rotating a full carousel, pivoting an individual joint, positioning a turntable, or guiding cables through the movement.
A tool carousel may combine a slewing ring or other rotary support with a geared drive, while individual magazine links may only pivot through a limited angle on plain bearings. Machine tending turntables may combine PRT slewing rings with drygear® drive technology, and moving utilities may require rotary e-chain® system. The DMG tool magazine application is a direct machine-tool example of repeated pivoting motion in a tool-handling system.

Customer Service:
Phone: Monday to Friday from 8 am - 8 pm
LiveChat: 24 hours
Book a Call
Book an Appointment with a Product Expert