Change Language :

There is no single best component for every application. Start with the load, the travel length, the required accuracy, the duty cycle, and the operating environment, then choose the guide and drive that match the actual motion rather than defaulting to what the last machine used. For supporting motion throughout a machine tool, common igus® options include drylin® linear guides and bearings for sliding and positioning movement, dryspin® lead screws where rotary motion must become controlled linear movement, and drylin® E motors and controllers where the movement needs to be driven. Primary cutting feed axes are a different class of system, selected around stiffness, feedback, and performance under cutting load, while igus® is strongest in the positioning, adjustment, and automation movement around them.
Linear motion appears throughout a machine tool, not only on the cutting axes. Machine guards and access doors slide open and closed, fixtures and stops are adjusted between setups, coolant and mist nozzles are repositioned, sensors and probes are set and reset, inspection equipment traverses the work area, and part handling systems load and unload the machine. Panels, drawers and service access points move as well, all relying on linear motion.
Usually the running surface, not the bearing body. Abrasive particles carried into a rolling system score the raceway and the rolling elements, which increases friction and clearance until positioning accuracy degrades and the assembly has to be replaced. Contamination-related failure tends to appear as gradually rising friction and lost precision rather than a sudden stoppage, which is why it often goes unaddressed until the machine is out of tolerance or an operator starts complaining that a guard or fixture has become hard to move.
In many cases, yes. Several drylin® series share the mounting dimensions of the recirculating ball bearing components they replace, so a worn or contaminated guide can be swapped for a dry-running one without redesigning the assembly around it. The replacement also removes what came with the original: the grease points, the lubrication lines feeding them, and the interval on the maintenance schedule. Where a standard part does not suit the existing geometry, components can be machined from tribologically optimized bar stock instead.
No. Recirculating systems need enough travel to circulate their rolling elements through the return path, which makes them a poor fit for short, frequent or oscillating strokes. Sliding bearings have no recirculation mechanism and therefore no minimum stroke, so they suit short-travel adjustment, fine positioning, and mechanisms that dither around a single point. This also makes them a practical choice for movements that happen rarely, since there is no lubricant to dry out, migrate or congeal between uses.
Lead screws suit adjustment, clamping, stop setting and positioning duties where the priorities are controlled movement, holding position and low maintenance rather than maximum thrust or high-speed traverse. They are also self-locking at appropriate lead angles, which means the mechanism holds its setting without a brake — useful on vertical adjustment, lift and tilt mechanisms. Thread form matters as much as the material: trapezoidal, ACME and high helix profiles each suit different combinations of speed, load and efficiency. For heavy continuous feed under cutting load, a ball screw remains the appropriate choice.
The deciding factors are how often the position changes, whether it needs to change during a cycle, and whether an operator can reach it safely. A hand-adjusted lead screw or sliding guide is appropriate for a setting made once per setup and left alone. A driven system earns its cost when the movement repeats, needs to be programmed, has to happen while the machine is running, or sits somewhere awkward to reach. drylin® E stepper, DC and brushless DC motors with matching controllers cover the driven case, with waterproof options available where coolant exposure is a factor.
Polymer sliding systems are generally the lower-cost option on component price, and the gap widens over the life of the machine, because there is no lubricant to buy, no lubrication hardware to install, and no servicing labor to schedule. Lightweight aluminum rails and shafts also cost less to ship and are easier to machine than hardened steel. The comparison that matters is not the price of the bearing but the total cost of the assembly around it, including the lubrication system the sliding version does not need.

Customer Service:
Phone: Monday to Friday from 8 am - 8 pm
LiveChat: 24 hours
Book a Call
Book an Appointment with a Product Expert